PLUS+1 User Forum
PLUS+1 Hardware => Controllers => Topic started by: macbahi on October 08, 2024, 11:30:21 PM
-
Hello,
I use Sc024-120 input C1p10 with APEM joystick TS6A1P00A use 5 Volt.
The joystick is Hall effect technology. It has 2 axis and one push button.
I connected it to C1P08 (Snsr_Pwr 5V) and the ground is C1P09.
First axe is connected as C2P1 and push button is connected to C1P10. The push button has ground configuration.
So my C1p10 bias is set to 1 as shown in image.
My problem is the push button don't work but when I use my voltmeter I see the push button working.
Please Have you idea what is my problem.
Thanks in advance for your help.
With best regards
-
Have you checked the voltage on the input in ServiceTool?
Voltage should be 5000mV and DigIn=0 when the button is off, and 0mV and DigIn=1 when the button is pushed.