Recent Posts

Pages: 1 2 3 [4] 5 6 ... 10
31
PLUS+1 Update Center / Missing Libraries
« Last post by Tor on March 18, 2025, 03:34:50 PM »
Hello,

In the latest version of PLUS+1 Update Center (v1.0.183) released with PLUS+1 Tools 2025.1.2 seems to have some missing libraries and files.
We don't know why, but troubleshooting is in progress.

We are sorry for any inconvenience.
32
Function Library / Re: SW Template flow
« Last post by Stefan on March 18, 2025, 02:27:36 PM »
Hello,

The way to use the template is to make sub-busses for e.g. CAN_Rx (see image).

When you want to connect to the bus you have created, e.g. CAN_Rx above, you have bring it out from the Main bus (see image).

I hope this will help to understand the template.

Have a nice day!
33
Function Library / Re: SW Template flow
« Last post by Lukey on March 18, 2025, 01:10:37 AM »
Personally I don't use the SW Template, I have my own style/template.

I've only seen the SW Template implemented once by another programmer and the 'flow' was a mess.

They don't even teach you to use the SW Template in any of the Danfoss training I have done...

Ultimately you are correct, you need to go backwards on yourself and tie the processed CAN information back to the Input bus so that you can use it else where;
Or just adjust the template as per your screen shots, there is no rules.

Also a good thing to know/remember is that the software processes GUIDE code differently, it isn't exactly left to right, search for 'About Execution Order' in the user manual (Press keyboard F1 button to launch the manual from GUIDE)
34
Off topic / Re: Attaching photos - 20k limit?
« Last post by jonbhanson on March 17, 2025, 08:49:32 PM »
I found that if I expand the "Additional Options..." checkbox, I have the option to attach files, and those attachments don't apply to the 20k character limit.
35
Function Library / SW Template flow
« Last post by jonbhanson on March 17, 2025, 08:45:13 PM »
I appreciate the SW template, thanks to whomever created them.

However, I am a bit confused about the execution flow through the template.


Inside the Input page, there is a sub-page for receiving CAN data (clever use of the tin can for the icon, by the way!)
Assuming some data is received on the CAN bus that needs to be subsequently processed by the application, it seems likely that the data from the CAN page will need to flow to some process page within the top level application page.
My confusion is that there is not really a "proper" way to send the output of the CAN page to the input of the process page.  The data would have to flow either 1. backwards from the CAN page through the Main bus on the left or 2. out of the CAN page the InPage bus on the right and then backwards into the application page. 



I understand that technically this will work because data placed on a wire is immediately propagated to the other nodes on that wire, so page order is what matters for execution order.  However, it seems like a bad practice to have the signal feeding backwards so to speak when the general rule is for program flow to be left to right.

What would make more sense to me is that the Input sub-pages should feed their outputs into the inputs of the application pages. 



Am I missing something here?  How do applications that use this template feed signals from CAN Rx or other input pages to the application processes?

Thanks!
Jon
36
Off topic / Attaching photos - 20k limit?
« Last post by jonbhanson on March 17, 2025, 08:38:22 PM »
I've been trying to ask a question and attaching photos to ease the description.  I insert the images by copying and pasting them into the message compose window.  However, every time I try to submit, I get the error

"The message exceeds the maximum allowed length (20000 characters)."

How am I supposed to attach a couple images to my question when there is a 20k limit?
37
PLUS+1 GUIDE CANKing / Re: Canking_problem
« Last post by Tor on March 13, 2025, 06:45:44 AM »
Hi,

Yes, I believe G3ORG3 is correct, but I don't think you need to reinstall it.
You can right click on the .exe file and go in to preferences and make it always start with admin rights.
I don't have CANKing installed but found below image online.

Have a nice day.
38
PLUS+1 GUIDE CANKing / Re: Canking_problem
« Last post by G30RG3 on March 12, 2025, 06:55:26 PM »
What windows version are you using?
Seems to me the install didn't go as planned. Do you have Admin rights on that computer?
I would try to reinstall with admin rights, and a turned down Anti-virus
39
PLUS+1 GUIDE CANKing / Canking_problem
« Last post by macbahi on March 12, 2025, 04:37:38 PM »
Hello,

I just installing Canking.  When I start it.  I get the message showing in the image enclosed.

Thanks in advance for your help.

With best regards
Mac bahi
40
Displays / Re: DM430E compile issues, error 446
« Last post by Tor on March 11, 2025, 06:40:26 AM »
Hi,

I'm sorry.  I guess there was a bit more at the end that shouldn't be there:
https://www.danfoss.com/en/campaigns/dps/plusplus1-support-form/

By the way.
You can always find the link to PLUS+1 Helpdesk in all the tools.  Help > Support > PLUS+1 Support Webpage.
In PLUS+1 Update Center there is a link on the right side after clicking "Select files manually".


Have a nice day.
Pages: 1 2 3 [4] 5 6 ... 10