Recent Posts

Pages: 1 ... 8 9 [10]
91
Controllers / Re: OutpuMode modification needed
« Last post by Lukey on November 15, 2024, 01:25:02 AM »
It is possible to change the output mode during operation.

I have successfully change between output mode 1 & 2.
This allowed me to drive a PNP and NPN (Sink and Source) wired relays from the 1 output.
That gave me 2 outputs from the 1 output, excellent for controlling a 2 way DCV for example.
92
Controllers / Re: OutpuMode modification needed
« Last post by macbahi on November 14, 2024, 08:53:32 PM »
Hello again,

It's done compilation without using switch I just put both DigOut and DutyOut not connected.

but I am not sure if this way is safe.

I will give the news soon.

With best regards
93
Controllers / OutpuMode modification needed
« Last post by macbahi on November 14, 2024, 07:53:58 PM »
Hello,

In the past I have change InputMode to use 2 mode in the same input and same project.  It's done with help from Sir Matt_Eng and Sir Tor (thanks another time).
You can see my topic link in the end of this message.
 
But now I want to change the OutputMode.  Because I want to use Output C2P03  one time as Sink Mode 2 and one time as PWM mode 3.   Please is it possible to do that?
My problem is in Output configuration page, Digout must one time connected to False and one time not.  And DutyOut one time connected to 0 (U16) and one time not connected.
Please have you any idea to do that.

Thanks in advance
Hamid
https://www.plus1forum.danfoss.com/index.php?topic=1525.msg5109#msg5109
94
Controllers / Re: Two PVEs on a single OX24-110 pin
« Last post by Camox on November 14, 2024, 08:45:11 AM »
Thank you for your answers.
Have a nice day!
95
Controllers / Re: Two PVEs on a single OX24-110 pin
« Last post by Lukey on November 14, 2024, 01:08:08 AM »
PVEA is Ratiometric yes, therefor I would bet Yes it should work fine with two coils on 1 output.

Regarding Active feedback or passive that shouldn't be a concern as is only related to the Fault Output of the PVE to Input of Controller.
96
Controllers / Re: Two PVEs on a single OX24-110 pin
« Last post by Camox on November 13, 2024, 02:41:35 PM »
We use active PVEA.
Thanks
97
Controllers / Re: Two PVEs on a single OX24-110 pin
« Last post by Lukey on November 13, 2024, 02:08:18 PM »
PVE Ratiometric coils?
I have not physically tried it but in theory it should work just fine, the output from the expansion module is only a reference voltage to the coil/s, there is no load, there shouldn't be an issue.
98
Controllers / Two PVEs on a single OX24-110 pin
« Last post by Camox on November 13, 2024, 12:16:08 PM »
Hello,
We need to add functionality to a second-hand machine equipped with an OX24-110 module.
The number of outputs available to control a PVE coil is insufficient.
I'd like to know if it's possible to control two PVE coils simultaneously with a single output. Have you ever done this?

Thanks in advance.
99
PLUS+1 GUIDE / Re: Project .p1x not found in folder
« Last post by dlewis on November 07, 2024, 02:41:59 PM »
So far 2024.3.5 works fine.
100
Displays / Re: DM430E flashing issue
« Last post by george on November 06, 2024, 04:39:34 PM »
Thank you sverreo for your suggestion. It helped to re-flash the display.
I didn't realise I need to add a third node on the system in order to complete the flash sequence as per Screenshot_4.png.

I added a second PEAK hardware with a different device ID and it allowed me to complete the flashing.

I will write a detailed instruction later for the benefit of others.
Pages: 1 ... 8 9 [10]