guys,
turns out that I have 3 non volatile memory on the application, it is in a DP570,
i input the values that i want to record, i can see that the value is there, then i cycle power, all came up with the recorded valeu but one.
one shows 65535 - because it is a u16 type, I do not understad why this happens
now assuming my logic is wrong I set the memory value with the service tool at dowload to 0, when it powers up I see 0, if I cycle power then I see again 655535, it only happens to 1 memory of 3 that I have.
does anyone knows what could be the issue?
Thanks I appreciate the feedback