Author Topic: Scripting through an update!  (Read 3147 times)

Offline Egholm-Jonas

  • PLUS+1 User
  • **
  • Posts: 6
  • Karma: +1/-0
Scripting through an update!
« on: January 07, 2025, 02:59:48 PM »
Hi,

I've tried several methods to ensure our dealers cannot take the wrong path or perform incorrect updates. However, I’ve noticed that if a dealer has a license and opens our application in design mode, they still have access to documents, resources and system navigator. :o

Is there a function I can call from the script to put their service tool into 'RUN mode' when eg. the '_ServiceTool_AfterFileOpen' function has been called?

Best regards,
Jonas

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 312
  • Karma: +28/-1
Re: Scripting through an update!
« Reply #1 on: January 09, 2025, 03:08:11 PM »
Hello Jonas.

There is a possibility to use the lock function (Design>Lock). This will at least hide the Design folder in both modes.    Unfortunately the Document folder is still visible.
The lock function can't be undone, so please create a backup!!

There is no way today to lock this with any script functions.

I think this will be a good feature, so I will add this to the PLUS+1 Wishlist.
Best regards,
Tor
PLUS+1® SW PAE Team