Hello,
I'm back with a new problem, which is the following
I want to test the reception of a can message to light a bulb when C1P06 is at 12 Volt
with CAN Monitor from the service tool, I can clearly see byte 7 changing state if C1P06 is at 12 volts, but the lamp does not light up
if with my network analyzer I send 80 to byte 7 of my frame with ID 0x100, my lamp lights up
so my reception part works if I send the frame myself!
the tx part of my program also works because I see it in CAN monitor of Service Tool
so everything is good but it doesn't work
I don't understand can you help me
thank you
Pat