Author Topic: ERROR 587  (Read 15937 times)

Offline hleppero

  • PLUS+1 Novice
  • *
  • Posts: 1
  • Karma: +0/-0
ERROR 587
« on: April 20, 2024, 06:14:45 PM »
I am getting this on a project after updating to 2024 version
*** ERROR 587 *** [PLUS1_IDE] INTERNAL: Unexpectedly reached else in {TXmifPresenter.GenerateOutput}
Same project was working fine in 2023 version. What is wrong?

Offline Camox

  • PLUS+1 Expert
  • ****
  • Posts: 62
  • Karma: +5/-0
Re: ERROR 587
« Reply #1 on: January 20, 2025, 05:06:16 PM »
Hello,
I have the same errors after little modifications in a software.
Do you have a solution ?

Guide version : 2024.4.3

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 312
  • Karma: +28/-1
Re: ERROR 587
« Reply #2 on: January 21, 2025, 07:36:13 AM »
Hello,

I have looked through some of the cases with this "Error 587" but have not come to any conclusion with only the information provided.

Some things to test. Please do a back up first!
1) Check if there are any non latin characters in the project path.
2) If the project is located in a synced network folder (OneDrive), please copy it it to a local folder and compile. If it's a Display project, the build folder (introduced in v2023.3.3) might be in a synced folder (GUIDE > Setup > Options > Compilation, look at the build folder path). If changing the path, copy the existing path in case you want to go back.

If this doesn't help, please contact PLUS+1 Helpdesk: https://www.danfoss.com/en/campaigns/dps/plusplus1-support-form/?plus1_product=guide
They will probably ask for the application to do some test.

Have a nice day.
Best regards,
Tor
PLUS+1® SW PAE Team

Offline Camox

  • PLUS+1 Expert
  • ****
  • Posts: 62
  • Karma: +5/-0
Re: ERROR 587
« Reply #3 on: January 21, 2025, 08:35:08 AM »
Hello Tor,
Thank you for your response.
I found a solution by creating a new project and copying the contents of the program in error.

For information, this is a project I've been working on for several weeks and the path is identical.

Have a nice day!
« Last Edit: January 21, 2025, 04:10:17 PM by Camox »

Offline Camox

  • PLUS+1 Expert
  • ****
  • Posts: 62
  • Karma: +5/-0
Re: ERROR 587
« Reply #4 on: March 06, 2025, 01:51:18 PM »
I'm replying to this post following new occurrences of this error.
After a request to support, the problem has been solved by deleting characters such as accents in the Guide project path.

I hope this helps.
Have a nice day!