Author Topic: Ackermann Function Block  (Read 11724 times)

Offline Pascal

  • PLUS+1 Novice
  • *
  • Posts: 3
  • Karma: +0/-0
Ackermann Function Block
« on: October 09, 2019, 03:36:34 PM »
Dear all,
Anyone already used Ackermann function block ?
What's happening when the whidth is bigger than the lenght, is that an issue ? I need this because our vehicle goes left side and right side only. Although the Max Wheel Angle in input of the FB is 4500 (45°) and the measure can not go more than 1800 (18°) ! moreover the outside steering wheel has an angle bigger than the inside wheel !
Could you help me ?
Thank you.
Pascal.