Hi Team,
I'm fairly new in PLUS+1 and whole this field. So sorry if this is a stupid question...
I have DM430 and trying to do a simple reading off the MBS 1250 on the display gauge.
Hardware:
1x DM430E-0-0-1-0
1x MBS 1250 0-250bar (063G1422)
I'm using a Functional blocks for MBS 1250 connected like this:
Input = Pin 6 (DigIn/AnIn) set up as per MBS manual:
n/a Bias
n/a Range
3000 DigThresHigh
2000 DigThresLow
Pin 8 = DigIn/AnIn using as 5V supply Pin 8-Snsr_Pwr
First question:
Can I use Pin 8 DigIn/An as my "Snsr_Pwr"? I saw there is a version of DM430 (DM430E-2-0-0-0) which is already having pin 8 define as Snsr_Pwr. Looking inside the program for this pin and comparing Pin.08_DigIn/AnIn and Pin.08_Snsr_Pwr, both have Voltage in it.