Author Topic: Viewing subpages: What do you think?  (Read 22331 times)

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 352
  • Karma: +8/-0
    • Marbek Elektronik
Viewing subpages: What do you think?
« on: September 20, 2012, 06:16:59 PM »
I wish, it would be possible to view inside the Sauer-Danfoss modules/pages.
It is OK, that it is not possible to make changes there.
But it would be better, I can see, what is inside.

What do you think?
Maybe Sauer Danfoss let us see inside?

Best regards,
Bernd
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
Re: Viewing subpages: What do you think?
« Reply #1 on: June 26, 2013, 02:11:19 PM »
Nobody wants to know, what is inside?
I want to look inside and perhaps take ideas for my programming.
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline 240glt

  • PLUS+1 Developer
  • ***
  • Posts: 35
  • Karma: +1/-0
Re: Viewing subpages: What do you think?
« Reply #2 on: June 26, 2013, 04:12:34 PM »
I agree, I would like to look inside also! That would also help to understand how to use some of the pages.

Offline dlewis

  • PLUS+1 Guru
  • *****
  • Posts: 110
  • Karma: +2/-0
    • Getman Corporation
Re: Viewing subpages: What do you think?
« Reply #3 on: June 26, 2013, 04:43:36 PM »
Looking inside would be helpful when an error message points to a location in a locked page.

Offline Daniel

  • PLUS+1 Expert
  • ****
  • Posts: 74
  • Karma: +6/-0
Re: Viewing subpages: What do you think?
« Reply #4 on: August 07, 2013, 08:35:23 AM »
Hi PLUS+1 users

Thank you very much for your inputs.
This has now been taken into consideration by the developers.


Best regards
Daniel
PLUS+1™ HelpDesk
PLUS+1® Help Desk Team

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 352
  • Karma: +8/-0
    • Marbek Elektronik
Re: Viewing subpages: What do you think?
« Reply #5 on: April 28, 2015, 12:41:51 PM »
Ok, now it is 2 years ago........
I have used J1939 function blocks - so far, so good.
But now I have to send this messages to another controller,
means: reading PGN and send the 8byte-array to another controller.
I will use for each PGN another ID and so on.

But now I can't use the danfoss function library, because it is closed and I can't get the array of 8 bytes.

So I have to write my own modules and delete the danfoss modules.

I wish, the would open their modules for reading and perhaps for modifying. They could make a automatic notice, so everybody could see, that this module is changed by the software-engineer.
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung