Author Topic: usb pen_drive connected to the 7 pin binder connector of display Dp620  (Read 14056 times)

campodavila

  • Guest
Hello every one, Can sameone helpme:
with a display dp620  I am trying to connect a usb pen_drive to the 7 pin usb connector for to save information(speed, rpm,etc),
is possible to do it  with this display?

In the Display librarys I have found the functions: Read_Applog and Write_USB , but  i can not get the components
"Define_Aplication_Log_Areas_Page"  and  "Define_Aplication_Log_Page that are necessary for to do it, it's as if these two components are not activated

thanks a lot
jose



Offline BRIan

  • PLUS+1 Expert
  • ****
  • Posts: 61
  • Karma: +3/-0
Re: usb pen_drive connected to the 7 pin binder connector of display Dp620
« Reply #1 on: September 26, 2013, 12:24:45 AM »
It is not possible with the DP6xx as there is no USB host facility.
BUT, the new DP6xxLX does have USB host function and there are new function blocks to make transfer easy-as, and a new cable ready made to accept the USB stick. Having said that, some USB sticks I've tried don't work.

campodavila

  • Guest
Re: usb pen_drive connected to the 7 pin binder connector of display Dp620
« Reply #2 on: October 01, 2013, 03:22:53 PM »
thanks Brian.
I will buy a dp620lx, but I have not clear how to put in the "Define_Aplication_Log_Page" the data that y need to log,
¿do you have a example?

thanks a lot ¡¡