Dear PLUS+1
® Users!
Danfoss Power Solutions is proud to announce the release of
PLUS+1® GUIDE and Service Tool version 9.0!
Determined to make PLUS+1
® GUIDE and Service Tool the #1 systems development tools for mobile hydraulic machinery, our PLUS+1
® Platform Development Team is driven to help you bring more-advanced, higher-performing, and better-quality machines to market even faster and easier!
Primary feature additions in this release (see the Release notes for more detailed information):C in GUIDE- New POU type for C Code
The C Code POU’s operate in a similar fashion to our Structured Text POU’s, but
allow the developer to write in native C code. The most useful application for these POU’s will be single C functions that can be contained within the POU and do not rely on other C resources.
- Direct import of .c and .h files
The C Code POU can also
call outside functions that are located in native .c files. GUIDE will prompt you to make a header file (.h) available to your POU. The .c file can contain one or many C functions that can also be called by other POU’s.
- Other added functionality is Syntax highlighting, Auto-completion, Parameter hints, Search in C POUs and .c/.h files, Debugger support
Display Editor Enhancements- Non-Modal Vector Based Screen Editor with tabs
The non-modal editor simply means that you can
work in both the GUIDE code editor and the screen editor at the same time. This is a big productivity enhancement for users with two monitors!
- Tabbed Editor
The screen editor now allows for
multiple screen definitions to be open within a single editor window in a tabbed format. Again, this is a big productivity enhancement so users can keep multiple screens open.
- Search and Replace
Arguably the biggest improvement to the screen editor is the addition of the search and replace. You can now easily
search through your project for screen content (fonts, text, images, etc.) and most of it
can even be replaced. This means that if you want to swap out an image that is on several different screens, you can now do it in a single operation. This is a big time saver!
Application LogIt is now possible to save Application Log 2 contents to USB stick in a faster way using the application log editor interface (requires HWD support).
Search- The search dialog can be shown in two views; vertical and horizontal.
- Improvements as buttons to expand/collapse all in search item tree, search item tree remembers its state, result can be exported to .csv or sorted into tabs and more.
- Search for PLC data types and constants has been added.
The
Module Viewer and the Compare SCS tools are now implemented as standalone executables. This reduces the memory usage of PLUS+1
® GUIDE.
License model updates- A license with an active maintenance period is now required. Existing pre-8.1 users will receive updated license keys via email.
- Perpetual Add-On licenses are no longer supported.
Download this new release
here where you can also find our detailed Release notes.
Best regards
Nilla
PLUS+1
® Helpdesk team